AnsweredAssumed Answered

Serialization with axi_ad9122.

Question asked by Jetmiri on Feb 24, 2015
Latest reply on Mar 16, 2015 by rejeesh

Hi all,

 

I am trying to use the axi_ad91122 with parameter Serdes Ddr N = 0. I don't want to make serialization of the input data since I want to send data with the same rate from the input to output of axi_ad9122. My input data rate at axi_ad9122 is at 16 MHz.

 

Q1: Is this a good idea to proceed, or there might be any other option!?

 

Q2: When I am putting the parameter Serdes DDR N = 0 I am seeing a warning after implementation saying that timing constraint are not set. Do I have to change anything else from the parameters!?

 

On the constraint file I already changed the input clock to axi_ad9122 to 16 MHz.

 

Regards,

Jet

Outcomes