AnsweredAssumed Answered

ADV7511 video inputs accept logic levels from 1.8 V to 3.3 V?

Question asked by ahamilton on Feb 24, 2015
Latest reply on Feb 24, 2015 by ahamilton

Although I have found the statement in the subject (video inputs accept logic levels from 1.8 V to 3.3 V) in the datasheet and elsewhere, I do not see how to do this.  The only electrical specifications I can find seem to indicate that the IO voltage can only be 1.8V because it is common to the core voltage.  My application requires that the video inputs be 2.5V.

Outcomes