AnsweredAssumed Answered

4xHDMI Rx to HDMI Tx with PIP capabilities.

Question asked by FreddyS on Feb 23, 2015
Latest reply on Mar 16, 2016 by DominicB

 

Hi,

My customer needsto design a box with the below features:

4 HDMI INPUTS 1080p 

1 HDMI Output to 55" screen 4K 

The box should control the output to the screen by mean of:

 

  • 1 of the inputs is seen on the full screen or
  • 2 of the inputs,are seen on the screen, each on 1/2 screen or
  • All 4 inputs are seen in the screen, each on 1/4 screen.

  

Please advise which chip or set of chips will be able to provide those features.

  Thanks

Freddy

Outcomes