AnsweredAssumed Answered

ADA4939-1 Pad Connection

Question asked by Joho Employee on Feb 18, 2015
Latest reply on Feb 19, 2015 by krisf

The question is about the ADA4939-1:

To which voltage level the exposed pad shall be connected?

Fig.53 in the datasheet indicates, that the pad is connected via 5 vias to a burried GND-Layer.

Nowhere else in the datasheet the recommended voltage level is mentioned.

 

Just to be sure: Can Analog Devices confirm that Fig. 53 is showing the correct voltage level connection of the exposed pad?

Outcomes