AnsweredAssumed Answered

AD9361 configured for swept measurements

Question asked by mlasher on Feb 17, 2015
Latest reply on Feb 23, 2015 by rgetz

I am in the process of evaluating the AD9361 to essentially replace our existing multi-block transceiver configuration. It would use one TX and both RX paths at the same time. The requirements are that it is able to be configured for full range (70MHz to 6GHz) sweeps with setup/settling/data transfer (single point measure) speeds of no greater than 2 mSec. After calibration of each of the LO frequencies is it possible to achieve point-point measurement speeds of 2 mSec?

Outcomes