AnsweredAssumed Answered

HMC244G16

Question asked by ADIguy on Feb 12, 2015
Latest reply on Feb 17, 2015 by s.ilke

Hello,

 

I'm performing a reliability analysis on the HMC244 for our application and require the following:

 

1.) On page 4 of the data sheet, marked 10 -119. The table for the  TTL/CMOS Control Voltages State Bias Condition Low 0 to +0.8 Vdc @ 5 uA Typ. High +2.0 to +5.0 Vdc @ 70 uA Typ. Do you have a maximum number for the current @ temperature?

 

2.) Do you have a maximum power dissipation spec for the device?

3.) Do you have Theta JC and Theta JA specs for the device?

 

Thanks and Best Regards.

Outcomes