AnsweredAssumed Answered

AD7719 crystal oscillator specification?

Question asked by sss on Feb 12, 2015
Latest reply on Feb 23, 2015 by sss

Hi all,

 

In the datasheet AD7719 , there is not crystal oscillator specification @32.768 kHz typ.

 

How value is following specifications?

 

Crystal oscillator specification

Logic Inputs, XTAL1 Only

VINL, Input Low Voltage: ? V

VINH, Input High Voltage: ? V

 

Crystal Equivalent Series Resistance:min/typ/max ? kΩ

Crystal Frequency:min ? /32.768(typ)/ max ? kHz

XTAL1 Input Capacitance: ? pF

XTAL2 Output Capacitance: ? pF

 

Best Regards,

sss

Outcomes