AnsweredAssumed Answered

ADXL362 Noise Density in Wake-Up Mode

Question asked by YuichiMASUDA on Feb 10, 2015
Latest reply on Feb 11, 2015 by YuichiMASUDA

Hi

 

I need detail information about Noise Density of ADXL362.

To decide threshold of motion detecting, I have two questions.

 

1. ODR of Wake-Up mode is 6Hz, but the ODR defined in BANDWIDTH is 12.5Hz to 400Hz.

Is it OK to calculate noise quantity using the 6Hz ODR?

 

2. Dose the Noise Density depend Temperature?

If it depends, I would like to know deviation at the operation temperature range.

 

Thank you.

Outcomes