AnsweredAssumed Answered

ADXL362

Question asked by nitin@anglia on Feb 10, 2015
Latest reply on Feb 10, 2015 by neilzhao

I am using an ADXL362 in an application. On the same physical hardware, it was previously consistently read sensible values (8bit). After various changes to the interfacing firmware, and then rolling back, it now reads (8bit and 12bit) as if it has a +1.66g offset applied to the X-axis. Is it possible that the firmware at some point overwrote a Reserved register value and in so doing has set a applied a permanent offset?

Outcomes