AnsweredAssumed Answered

"no section in the code memory space" when creating a loader file

Question asked by WaNa on Nov 12, 2010
Latest reply on Jan 12, 2011 by gvasanth

Hi,

 

I have a project for the BF512F which runs perfect with the emulator.

Now I want to download it to the internal Flash. For this I have to create a loader file.

I have selected the ADSP-BF512-ROM-V01.dxe as initialisation file in the project options : load : options.

When I create the project the tool gives me the following error message:

 

Creating loader file...
Error: no section in the code memory space
Tool failed with exit/exception code: 4294967295.
Build was unsuccessful.

 

I have no idea where the problem is.

Outcomes