AnsweredAssumed Answered

ADV7181C Color issue

Question asked by kbouhara on Feb 9, 2015
Latest reply on Feb 17, 2015 by kbouhara

Hi,

 

We are working with ADV7181C and RGB GR mode (XVGA 1024x768) to output YCbCr 4:2:2. We have the following register setting (from adv7180.c hard_reset()): 

 

@

 

     adv7180_write_reg(ADV7180_INPUT_CTL, 0x00);

        adv7180_write_reg(0x05, 0x02); //;Prim_Mode =001b COMP

        //if(video_idx = ADV7180_SVGA) {

        //      adv7180_write_reg(0x06, 0x01); //;VID_STD=1010b for 720P 1x1

        //} else if (video_idx = ADV7180_XGA) {

        adv7180_write_reg(0x06, 0x0c); //;VID_STD=1010b for 720P 1x1

        adv7180_write_reg(0x1D, 0x47); //;Enable 28MHz Crystal

        adv7180_write_reg(0x3A, 0X21); //;set latch clock settings to 010b, Power Down ADC3

        adv7180_write_reg(0x3B, 0x81); //;Enable Internal Bias

        adv7180_write_reg(0x3C, 0x5D); //;PLL_QPUMP to 101b

        adv7180_write_reg(0xC3, 0x56);//ADC1 to Ain5, ADC0 to Ain6,

        adv7180_write_reg(0xC4, 0xB4);//ADC2 to Ain4 and enables manual override of mux

        adv7180_write_reg(0x6B, 0x83); //;Select 16 bit YPrPb out from CP

        //adv7180_write_reg(0x85, 0x03); //;Turn off SSPD and force SOY. For Eval Board.

        adv7180_write_reg(0x86, 0x0b); //;Enable stdi_line_count_mode

        adv7180_write_reg(0xBF, 0x06); //;Blue Screen Free Run Colour

        adv7180_write_reg(0xC0, 0x40); //;default color

        adv7180_write_reg(0xC1, 0xF0); //;default color

        adv7180_write_reg(0xC2, 0x80); //;Default color

        adv7180_write_reg(0x0E, 0X80); //;Enable Hidden Space.

       //adv7180_write_reg(0x52, 0x46); //;Enable SOG/SOY Clamp Filter

        adv7180_write_reg(0x54, 0x00); //;CML Level Change

        adv7180_write_reg(0xF6, 0x3B); //;ADI Recommended Setting

        adv7180_write_reg(0x0E, 0x00);// ; Disable Hidden Space.

        adv7180_write_reg(0x0E,0x80);//ADI Recommended Setting

        adv7180_write_reg(0x52,0x46);//ADI Recommended Setting

        adv7180_write_reg(0x54,0x00);//ADI Recommended Setting

        adv7180_write_reg(0x0E,0x00);//ADI Recommended Setting

        adv7180_write_reg(0x52,0x80);//ADI Recommended Setting

        adv7180_write_reg(0x57,0x08);//ADI Recommended Setting

        adv7180_write_reg(0x5B,0x20);//ADI Recommended Setting

        adv7180_write_reg(0x5C,0x00);//ADI Recommended Setting

        adv7180_write_reg(0x62,0x00);//ADI Recommended Setting

        adv7180_write_reg(0x63,0x01);//ADI Recommended Setting

        adv7180_write_reg(0x67,0x03);//ADI Recommended Setting

        adv7180_write_reg(0x68,0x01);//ADI Recommended Setting

        adv7180_write_reg(0x7B,0x1D);//TURN OFF EAV & SAV CODES Set BLANK_RGB_SEL

        adv7180_write_reg(0x8f, 0x02); //;XVGA HSync Clock

        adv7180_write_reg(0x90, 0x50); //;XVGA HSync Clock

        adv7180_write_reg(0x7e, 0xa0); //;XVGA VESA H Back Porch 160pixels

        adv7180_write_reg(0x7d, 0xa0); //;XVGA VESA H Back Porch 160pixels

 

With this, we don't have a correct color image and we have tried several csc setting from ADV7181C_ADV7181C@_ADV7341-VER.3.2c.txt but without success ...

Question is, what do we have to set for RGB -> YCrCb conversion ? Are we missing something ?

Attachments

Outcomes