AnsweredAssumed Answered

Can ADuM4160 Detect Device Removal Event as A Peripheral?

Question asked by diverger on Feb 7, 2015
Latest reply on Feb 18, 2015 by MMA

In ADI's reference design CN0160, the "USB Peripheral Isolator Circuit", if the peripheral is disconnected from the upstream port (that is, remove from the host), if the downstream can detect the event? Or I have to use other method to detect the Vbus removal event?

Attachments

Outcomes