AnsweredAssumed Answered

indoor navigation with ADIS16305?

Question asked by ADI@EBV on Feb 2, 2015
Latest reply on Feb 11, 2015 by NevadaMark

I have to solve the following problem:

The x-y-z-coordinates of a box in a closed and shielded hall (100m x 100m x 15m) have to be monitored (data-tranfer via wireless-modul to a central unit). Position accuracy needs to be about 10..20cm.

Is it possible to build up a system with e.g. ADIS16305, which could fulfill the requested needs?

Because I am rather un-experienced with this kind of navigation stuff, I am interested in app-notes etc., which could help me in

setting up a possible solution.

Thanks in advance!

BR, Dirk

Outcomes