AnsweredAssumed Answered

KC705+AD-JESDADC1 connection

Question asked by superco on Feb 1, 2015
Latest reply on Feb 11, 2015 by charlyelkhoury

Hi all,

I apologize if my question is redundant. I am a newbie on this field..

I am trying to transmit my waveform through the AD9129 DAC(on FMC-176 board) + KC705.and to digitize it via AD9250 on the same board.

My plan is to use the iio-oscilloscope remotely for the setting it up, loading, and capturing my waveform.

 

1. So my first question is whether the prebuilt AD-jesdadc1 image ((http://swdownloads.analog.com/cse/2014_r2_pre/kc705_fmcjesdadc1_2014_R2_PRE.zip) supports AD9129 DAC like the reference design does(ADI AD-FMCJESDADC1-EBZ Boards & Xilinx Reference Design [Analog Devices Wiki])? if not, what should I do to make it work with the DAC? I do not see the linux driver for it...

 

2. Second question is that after I programmed the image on KC705, and it shows the obtained ip address on the display,

the remote iio-oscilloscope (the latest compiled one that I use to connect to another zedboard) says that the device is not found. I wonder if there's any version compatibility between the image and iio-oscilloscope?

Outcomes