AnsweredAssumed Answered

Two ADE7878A's - one MCU

Question asked by gtrue1978 on Jan 30, 2015
Latest reply on Feb 5, 2015 by gtrue1978

Hello,

 

We are running tests using the ADE7878A evaluation board with the goal of having the ADE7878A on a future product. Currently, we are wondering whether or not it is possible to have 2 ADE7878A´s on the same board and communication through I2C with a single MCU.

 

As far as I could understand from the ADE7878A user manual, it has always the same 0111000 slave address. Well, if I cannot changed it, I cannot distinguish between both of them using the same bus.

 

Am I understanding this properly? Is there anyway to change the I2C slave address in the ADE7878A?

 

Thank you!!

Outcomes