AnsweredAssumed Answered

ADV7511 in 2560x1080p

Question asked by williamcumby on Jan 29, 2015
Latest reply on Feb 12, 2015 by DaveD

Can the ADV7511 be configured to drive 2560x1080p?  The pixel clock would be too high at 60Hz frame rate.

Would one of the following be possible?

 

86 1080p24   64:27    1:1        2560x1080p @ 23.98/24 Hz

87 1080p25   64:27    1:1        2560x1080p @ 25Hz

88 1080p30   64:27    1:1        2560x1080p @ 29.97/30 Hz

89 1080p50   64:27    1:1        2560x1080p @ 50 Hz

 

Thanks!

 

--Will Cumby

Outcomes