AnsweredAssumed Answered

Op amp recommendation

Question asked by jamesa on Jan 27, 2015
Latest reply on Jan 29, 2015 by AnnaFeB

I need an op amp in a DIP package for a circuit with the following characteristics:

- 24 vdc filtered and regulated power supply (can install 24 vdc to 5 vdc converter if necessary)

- industrial instrumentation application

- voltage follower (unity gain) with switching occurring at once a minute (max)

- high resistance (megohms) dc voltage divider input to op amp

- op amp input voltage would be 0 or 24 vdc with 24 vdc power supply or 0 or 5 vdc with 5 vdc power supply

- op amp load is 2600 ohms (approx 1 ma)

- op amp could be subjected to 40 degC.

 

Thanks in advance

Jim

Outcomes