AnsweredAssumed Answered

Issue with Linux Nano-Distribution on Zynq (with FMCOMMS2)

Question asked by Quamstar on Jan 27, 2015
Latest reply on Feb 6, 2015 by larsc

Hey Guys,

 

as discribed in several Forums and Topic it might be possible to run any linux distrubution on zynq (ref: Installing Linux on Zedboard | Zedboard). As discribed on Zynq and the AD9361 and/or AD9364    [Analog Devices Wiki] you can install the rootfile system on a ext4 format partition on the sd-card. Following that instruction everything works fine (for this version - 12.11). When i try to install another rootfile-system, for example the newest release of linaro nano 14.12 (Linaro Releases) i receive the following error:

 

#0: HDMI monitor

#1: ZED ADAU1761

EXT4-fs (mmcblk0p2): recovery complete

EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)

VFS: Mounted root (ext4 filesystem) on device 179:2.

devtmpfs: mounted

Freeing unused kernel memory: 196K (c05c6000 - c05f7000)

request_module: runaway loop modprobe binfmt-0000

Starting init: /sbin/init exists but couldn't execute it (error -8)

Starting init: /etc/init exists but couldn't execute it (error -13)

request_module: runaway loop modprobe binfmt-0000

Starting init: /bin/sh exists but couldn't execute it (error -8)

 

This happens with many other distribution (outstanding the 12.10 and 12.11 like discribed on the wiki)

 

it seems that the kernel panic for a reason that i cannot explain by my self. Do you have any idea what goes wront?


By the way i use the newest kernel of the 2012_R2 branch (https://ez.analog.com/message/167891#167891) as well as the devicetree file

 

I hope you can help me with this issue

 

Thanks and regards
Jan

Outcomes