AnsweredAssumed Answered

Hello

Question asked by olaffromstendal on Jan 27, 2015
Latest reply on Jan 27, 2015 by ColemanR

i have to update 160 Computer from XP to W7 64.

After Installation a sound driver from Asus:

ADI 1988A/B Audio Driver v6.10.X.6585 for XP / Vista / Win7 32bit and 64bit, there is an bad electrically background noice. With W764 standard driver not.

In addition Mixer and Line are not available.

I need Mic an Mixer (or Line) at the same time!

Is there a new driver or some ohter helpful infomation for me.

Thanks.

Outcomes