AnsweredAssumed Answered

ADP1741ACPZ-R7 dropout voltage

Question asked by Belenie on Jan 27, 2015
Latest reply on Feb 5, 2015 by Belenie

Hello,

 

For analog Devices ADP1741ACPZ-R7 the datasheet specifies the dropout voltage for conditions when Vout is 1.8V or higher as 280mV max on page 3 (although footnote 4 actually says for when Vout is 1.6V or higher). The datasheet also shows the dropout voltage verses load current for both Vout = 1.6V and Vout = 2.5V in Figure 12 on page 8.

 

In my application, my Vout = 1.3V and I would like to know what my dropout voltage is @ 2A. It would be nice to see a graph as shown in Figure 12 but I would be happy with just knowing the worst case dropout with Vout = 1.3V and 2A load current.

 

Thanks,

Belenie

Outcomes