AnsweredAssumed Answered

AD9361 Linux driver tuning without TX wired up

Question asked by njp on Jan 26, 2015
Latest reply on Nov 14, 2015 by DragosB

Hi,

I have a custom board where I am only using the receive path and the TX pins are not wired to the FPGA. Because of this, I've had to make some changes to ad9361.c (attached) to get it to work, because the TX tuning understandably fails. I also use TDD mode.

I just pulled the most recent kernel, and it looks like the "Improve TX QUAD CAL" commits are again giving me issues. I'm just going to not merge in these specific changes for now, but if possible it would be nice if the driver worked in an RX-only setup.

Outcomes