AnsweredAssumed Answered

ADV7511: Image shifted and cropped

Question asked by d.s.e on Jan 23, 2015
Latest reply on Jan 28, 2015 by GuenterL

Hi,

 

I really have a problem to get a proper output from the ADV7511.

The input ist 720p @ 50 Hz, but the monitor connected via DVI says, it's 720x480.

Also the image is shifted to the right, and the displayed part is only the top left part of the whole image (see attached image).

 

any hints?

Outcomes