AnsweredAssumed Answered

AD9910 Impedance matching with Balun

Question asked by FreddyS on Jan 20, 2015
Latest reply on Dec 13, 2017 by LouijieC

 

Dear Supporter,

Suppose I want to use the AD9910, according your recommendation in AD9910 impedance matching

with a balun transformer that have 1:1 loop ratio, and I would like to match it to a 50Ω load.

Can I use only two 25Ω resistors, each connected to DAC output ?

 

Are there better matching options for such case ?

 

cid:image005.png@01D02D88.030696B0

 

Thanks

 

Outcomes