AnsweredAssumed Answered

ADuM4160 internal clearance?

Question asked by Jim-E on Jan 19, 2015
Latest reply on Jan 21, 2015 by Jim-E

Hi.

 

What is the internal clearance between the isolated sides on the ADum4160 iCoupler?

Since the Rated Dielectric Insulation Voltage is 5000V I would assume that the internal clearance is more than 0.017mm or is it actually so small?

I am searching for an USB isolator that that would have >0.2mm internal clearance. (iec60079-11, Table 5).

 

Br.

Jim

Outcomes