AnsweredAssumed Answered

Install linux to run on VC707 Microblaze AD-FMCOMMS3-EBZ AD9361 build?

Question asked by AnhDat on Jan 16, 2015
Latest reply on Feb 2, 2015 by DragosB

I'm missing a step in the documentation I think.

It appears (even though some of the pages don't have linux as an option for the VC707) that it is since the reference designs runs a linux kernel I should be able to get it up and running as well, correct?  But there is no check for VC707 on "Linux Software" at AD-FMCOMMS2/3/4/5-EBZ Quick Start Guides [Analog Devices Wiki] - does that need to be updated?

Following steps:

1- I do my own vhdl build following from the latest git repo- ADI Reference Designs HDL User Guide [Analog Devices Wiki]

2- But when I go to follow AD-FMCOMMS2-EBZ / AD-FMCOMMS3-EBZ / AD-FMCOMMS4-EBZ / AD-FMCOMMS5-EBZ Linux support [Analog Devices Wiki] I'm a bit stuck - I try to follow http://wiki.analog.com/resources/tools-software/linux-drivers/iio-transceiver/ad9361

 

but basically where is how to get the linux kernel compiled on the microBlaze, I guess using SDK?

do I have to do a baremetal - no-OS install first following AD9361 No-OS Software [Analog Devices Wiki] ...

 

Thanks!

Outcomes