AnsweredAssumed Answered

Need help with SigmaStudio3.2 & EVAL-1701MINIB Active Download.

Question asked by Raydon on Nov 5, 2010
Latest reply on Nov 5, 2010 by Raydon

I am working with SigmaStudio3.2 & EVAL-1701MINIB connected via USBi.  When I select "Link Compile Download" the schematic status bar below the work space turns green and "81% Active Downloaded"  is displayed in the application status bar.  I tried loading another project (that worked previously) and could only get to "90% Active Downloaded".  Can anybody help?  I have re-booted my pc and re-installed SigmaStudio. I am at a complete loss here.  Any suggestions would be greatly appreciated.

Ray

Outcomes