AnsweredAssumed Answered

Questions regarding ADAU1979

Question asked by catalin.dumitrescu on Jan 15, 2015
Latest reply on Sep 19, 2017 by galvinpjg

I have a couple of questions regarding ADAU1979.
1) what is the value of the Vref used by the chip
2) when the chip is operating in slave mode (LRCLK pin as clock source) the MCLKIN pin should be left not connected or pulled to GND / VCC
3) how can I configure a sampling rate of 8kHz (is this done by setting the  FS field from SAI_CTRL0 register to 00 and the frequency provided by LRCLK ?)


Thank you for the help!

Outcomes