AnsweredAssumed Answered

how to use uCos with system service and drivers

Question asked by xuyejin@sina.com on Jan 15, 2015
Latest reply on Jan 18, 2015 by xuyejin@sina.com

HI,

    I use BF526,want to use uCos with system service and drivers in VisualDsp++ 5.0.

    but have some problem.

 

    in adi_int.c

$Revision: 5506 $

$Date: 2011-07-26 10:45:48 -0400 (Tue, 26 Jul 2011) $

 

 

Description:

            This is the source code for the interrupt manager.

 

 

            Note that one of the following macros must be defined.  These macros

            are used to include the proper implementation code for the specified

            operating environment:

 

 

                o ADI_SSL_STANDALONE    - no RTOS (standalone operating environment)

                o ADI_SSL_VDK           - VDK operating environment

                o ADI_SSL_THREADX       - ThreadX operating environment

                o ADI_SSL_INTEGRITY     - Integrity operating environment

                o ADI_SSL_UCOS          - uCOS-II operating environment

 

 

*********************************************************************************/

 

          where to define the ADI_SSL_UCOS macro ? to link the library libssl526_ucos.dlb?

          I trust some ways ,but can not to success。when I simulate,the software goto adi_int_standalone.c always.

 

          I have trusted to define  ADI_SSL_UCOS  in project option-> preprocessorEWA{G48]U%S5X1]F5B6@8U5.jpg

          in   project option-> link -> LDF processing ->Preprocessor macro

XNL[R@1V)1(A0L(FQ$R9VIO.jpg

      or in my files

    55G27K~2M366%PK9Q4AJ{17.jpg

      these dfines is not successed all.

 

           regards   yejin xu

Outcomes