AnsweredAssumed Answered

No Blackfin USB devices were found while running vat_file_io_adsp_bf609

Question asked by lalitha123 on Jan 14, 2015
Latest reply on Jan 22, 2015 by bijeshp

Hi

I was trying to run vat_file_io_adsp_bf609 example on BF609-EZKIT. I connected ADZS-HP-USB-ICE as emulator as given in the readme file. yet when I open the command prompt to hostapp_cces.exe but it says No Blackfin USB device devices were found. I kept SW2 in position 1 as given in the readme file but the code kept running indefinitely and was not showing "Opening USB device for STDIO..." in the output console. So I tried with SW2 at position 0 which ran and showed "Opening USB device for STDIO..." in the output console. Then in command prompt I ran hostapp_cces.exe which showed "No Blackfin USB device devices were found". Please help in solving the issue.

 

Thanks

Lalitha

Outcomes