AnsweredAssumed Answered

High Accuracy High Precision Gyro

Question asked by shrims4u@gmail.com on Jan 13, 2015
Latest reply on May 5, 2015 by NevadaMark

Hi,

 

1.     I have a huge metal block which rotates clockwise as well as anticlockwise. The speed of movement is not so high. However there is a huge shock which passes through the block sometimes.

 

2.     I need to measure the amount of angular movement in degrees of the metal block be it clockwise or anticlockwise.

 

3.     The accuracy I require is very high i.e. of the order of less than 5 minutes(1 degree/12). Also a high precision level is required.

 

4.     The cost limit onto me is Rs 50,000/- or less than $800 dollars.

 

Any help will be appreciated. Thanks.

Outcomes