AnsweredAssumed Answered

HMC1048

Question asked by TimW Employee on Jan 9, 2015
Latest reply on Jan 14, 2015 by enewman

Any cautions about reversing the connections on the RF & IF port?  Would like to use the device as an upconverter.

 

Output Freq (RF):   3.8GHz     |4.2GHz     |   3.8GHz       |   4.2GHz

 

Input Freq (IF) :  1.472GHz |1.472GHz |   2.45GHz     |2.45GHz

 

LO                       2.328GHz | 2.728GHz|1.35Ghz     |1.75GHz

 

 

Thanks,

Tim

Outcomes