AnsweredAssumed Answered

A suitable interface device for AD7762

Question asked by moto on Jan 7, 2015
Latest reply on Feb 6, 2015 by moto

Hi

I would like to select the suitable interface device, as level translator to 3.3V, for AD7762.

An interface device's Vinh min is mostly 0.7 or 0.65 X Vdd min, I think.

It is about 1.65V at vdd=2.5V.

But AD7762/3 's Voh is 1.5V min.

 

Could I select suitable interface device ,with a guarantee?

 

Regards

moto

Outcomes