AnsweredAssumed Answered

BF532 in SPI slave mode

Question asked by Ruslan on Nov 1, 2010
Latest reply on Nov 2, 2010 by Andreas

How possibly use of SPI slave method? Is the init code needed?

I cant compile any project with init code added:

Creating loader file...
Error: no section in the code memory space
Tool failed with exit/exception code: 4294967295.
Build was unsuccessful.


Example init code in EE240 have another problem:

Linking..

[Error li1021]  The following symbols referenced in processor 'p0' could not be resolved:
        'main [_main]' referenced from 'crtsf532y.doj

Linker finished with 1 error
cc3089: fatal error: Link failed
Tool failed with exit/exception code: 1.
Build was unsuccessful.

 

Now, after loading 10 bytes into BF pin PF8 goes to the Zero. I am load all program (without init code) but it cant start. PF8 stays Zero.

After selecting in ProjOptions Load -> SPI slave, binary and another flag, I cant see any changes in bytes 9-10 of *ldr file (0x: 10 00).

Is it possible use BF SPI slave mode?

Outcomes