AnsweredAssumed Answered

What RF/BW limitations to AD-FMCOMMS3-EBZ: AD9361 2 Rx + 2 Tx simultaneous streams?

Question asked by AnhDat on Jan 7, 2015
Latest reply on Jan 16, 2015 by rgetz

I just want to confirm the AD-FMCOMMS3-EBZ: AD9361 supports 2 Rx + 2 Tx simultaneous streams at one time that are both in similar RF ranges correct?  I was double checking the documentation and just wanted to make sure that all 4 transceivers may be independently tuned to separate RFs and bandwidths within the specs 70MHz to 6GHz with BW <200kHz to 56 MHz?  Or what are the limitations?

For example could one have a functional application with RF1-IN be 1 GHz, RF2-IN 1.5 GHz, RF1-OUT 2GHz, RF2-OUT 2.5GHz all with 50MHz BW operating simultaneously?

 

What limitations if any to the independence tuning ranges of the 4 transceivers?

 

THANKS!

Outcomes