AnsweredAssumed Answered

AD-FMCOMMS3-EBZ HDL for VC707 /hdl/tree/hdl_2014_r1/projects/fmcomms2/vc707

Question asked by AnhDat on Jan 1, 2015
Latest reply on Jan 1, 2015 by rejeesh

Goal: build the latest release/working HDL build for AD-FMCOMMS3-EBZ for VC707, OS or non-OS version with microblaze processor.

 

Issue: It error's out at start of build process using tcl scripts

 

Background/Details:

 

AD-FMCOMMS3-EBZ Quick Start Reference Design for VC707

 

I've been trying to get a working HDL build running following directions at AD-FMCOMMS2-EBZ / AD-FMCOMMS3-EBZ / AD-FMCOMMS4-EBZ HDL / AD-FMCOMMS5-EBZ HDL Reference Design    [Analog Devices Wiki] and ADI Reference Designs HDL User Guide    [Analog Devices Wiki] by pulling off of the release HDL branch hdl/projects/fmcomms2/vc707 at hdl_2014_r1 · analogdevicesinc/hdl · GitHub

 


WARNING: [BD 41-1306] The connection to interface pin /axi_spdif_tx_dma/m_axis_mm2s_tready is being overridden by the user. This pin will not be connected as a part of interface connection M_AXIS_MM2S

#### connect_bd_net -net sys_200m_clk [get_bd_pins sys_audio_clkgen/clk_in1] $sys_200m_clk_source

#### connect_bd_net -net sys_100m_reset [get_bd_pins sys_audio_clkgen/resetn] $sys_100m_resetn_source

ERROR: [BD 41-722] Specified net 'sys_100m_reset' does not exist. Please use an existing net name

ERROR: [BD 5-4] Error: running connect_bd_net.

ERROR: [Common 17-39] 'connect_bd_net' failed due to earlier errors.

    while executing

"connect_bd_net -net sys_100m_reset [get_bd_pins sys_audio_clkgen/resetn] $sys_100m_resetn_source"

    (file "../../../projects/common/vc707/vc707_system_bd.tcl" line 458)

    while executing

"source $ad_hdl_dir/projects/common/vc707/vc707_system_bd.tcl"

    (file "system_bd.tcl" line 2)

    while executing

"source system_bd.tcl"

    (procedure "adi_project_create" line 94)

    invoked from within

"adi_project_create fmcomms2_vc707"

    (file "system_project.tcl" line 7)

Outcomes