AnsweredAssumed Answered

External Reference Issue

Question asked by jfevold on Dec 31, 2014
Latest reply on Apr 27, 2018 by pwz

I followed all the directions to use an external reference found atFMCOMMS2 - external reference clock but I'm getting a few errors on boot and I can't display a signal in the oscilloscope.

 

ad9361 spi32766.0: Calibration TIMEOUT (0x247, 0x2)

ad9361 spi32766.0: Calibration TIMEOUT (0x287, 0x2)

ad9361 spi32766.1: ad9361_dig_tune: Tuning RX FAILED!

ad9361 spi32766.1: ad9361_dig_tune: Tuning TX FAILED!

 

I set the clock to 10MHz and plugged in a 10MHz reference clock. I removed the resistor and placed the capacitor per the instructions.

 

What could be the issue here?

Thank you

Outcomes