AnsweredAssumed Answered

Error while compiling for ADAU1452 under Sigmastudio

Question asked by Cape on Dec 22, 2014
Latest reply on Dec 23, 2014 by Cape

Dear all,

 

I'm trying to develop an audio mixer application with ADAU1452.

My project uses an input matrix (22x24), 12 processing channels and an output matrix (26x14).

When I try to compile the project Sigmastudio outputs the following errors:

 

error (1494,NxM Linear1): The name 'target_0_24' in memory 'DM0' is undefined in module NxNMixerSlewS300Alg1 (1964)

error (1495,NxM Linear1): The name 'gain_0_24' in memory 'DM0' is undefined in module NxNMixerSlewS300Alg1 (1965)

error (1753,NxM Linear1): The name 'target_15_24' in memory 'DM0' is undefined in module NxNMixerSlewS300Alg1 (2223)

error (1754,NxM Linear1): The name 'gain_15_24' in memory 'DM0' is undefined in module NxNMixerSlewS300Alg1 (2224)

error (1330,NxM Linear2): The name 'target_0_28' in memory 'DM0' is undefined in module NxNMixerSlewS300Alg2 (7586)

error (1331,NxM Linear2): The name 'gain_0_28' in memory 'DM0' is undefined in module NxNMixerSlewS300Alg2 (7587)

error (1405,NxM Linear2): The name 'target_15_28' in memory 'DM0' is undefined in module NxNMixerSlewS300Alg2 (7661)

error (1406,NxM Linear2): The name 'gain_15_28' in memory 'DM0' is undefined in module NxNMixerSlewS300Alg2

 

As far as I can understand, it seems that somewhere there are some parameters regarding ouput 24 of the first matrix and output 28 of the second matrix, but the two matrix are not that big.

Any idea on where I am failing?

 

Thank you very much.

Best regards.

Outcomes