AnsweredAssumed Answered

Need some ADV7401 Register Configuration Settings

Question asked by oliverfbrown on Dec 18, 2014
Latest reply on Dec 18, 2014 by GuenterL

 

We are using the ADV7401 on one of our boards and we would like to make sure that we have the correct register setting.

 

Do you have example for the following configuration.

 

 

 

1.       CVBS AIN-10 – NTSC/PAL 8-bit 422 Output (This should be the one on page 303 in the manual, ADV7401_Manual_RevB)

 

 

 

2.       CVBS AIN-10 – NTSC/PAL 16-bit 422 Output.

 

 

 

3.       720P YPbPr Input on AIN 6, 5 and 4 - 1x1 24-Bit 444 Output (This should be the one on page 311 in the manual). For this mode we may need to swap the YUV output channels. Is that possible? We also may want to use RGB instead of YUV how do we do that?

 

Outcomes