AnsweredAssumed Answered

ADV7611 0x72 Register Space

Question asked by mferraro on Dec 11, 2014
Latest reply on Dec 11, 2014 by mferraro

With EVAL-ADV7611EB1Z_scripts_v3_0 ; what is register space is 0x72 referring to?

Example: :6-1e Port A, 720p,1080i Any Color Space In (YCrCb 444 24bit from ADV761x) Through HDMI Out 444 YCrCb VIC[4,5,19,20]:

It does not show up in any of the remaps

 

 

98 FF 80 ; I2C reset
98 F4 80 ; CEC
98 F5 7C ; INFOFRAME
98 F8 4C ; DPLL
98 F9 64 ; KSV
98 FA 6C ; EDID
98 FB 68 ; HDMI
98 FD 44 ; CP
98 01 06 ; Prim_Mode =110b HDMI-GR

 

here is the piece of the 0x72 sequence

 

 

72 01 00 ; Set N Value(6144)
72 02 18 ; Set N Value(6144)
72 03 00 ; Set N Value(6144)
72 15 00 ; Input 444 (RGB or YCrCb) with Separate Syncs, 44.1kHz fs
72 16 70 ; Output format 444, 24-bit input
72 18 46 ; CSC disabled
72 40 80 ; General Control packet enable
72 41 10 ; Power down control
72 48 08 ; Data right justified
72 49 A8 ; Set Dither_mode - 12-to-10 bit
72 4C 00 ; 8 bit Output
72 55 40 ; Set YCrCb 444 in AVinfo Frame
72 56 08 ; Set active format Aspect
72 96 20 ; HPD Interrupt clear

Outcomes