AnsweredAssumed Answered

FMCOMMS 5 with Linux

Question asked by CMC-B on Dec 11, 2014
Latest reply on Dec 11, 2014 by CMC-B

I recently received an FMCOMMS 5 board, it was shipped with a SD Card containing various Boot Images  (SD Card is marked as "January 2014")

 

I am using a ZC706 board and configured the SD card to boot the "zynq-zc706-adv7511-ad9361" image.  With the FMCOMMS 5 installed, I can boot the system and get to the Ubuntu Screen and see the IIO applications in the left hand bar. 

 

When I run the IIO applications, however, they do not seem to detect the presence of the FMCOMMS 5 board, no devices are shown.  I also do not see the FMCOMMS5 plugin.  I have previously used this system with an FMCOMMS2 card successfully, albeit with an older boot image (which shipped with the FMCOMMS 2 card).

 

Is there a quick way to determine if the SD card that was shipped has the proper images?  or can you offer any other suggestions to get this board up and running?

Outcomes