AnsweredAssumed Answered

VDDA_GPO range

Question asked by rgetz Employee on Dec 11, 2014
Latest reply on Jan 6, 2015 by rgetz

Hi.

 

In Rev C of the AD9361 datasheet (let me know if I need to find a newer one). It says:

 

VDD_GPO Supply Nominal Setting is between 1.3 and 3.3V (the table in SUPPLY CHARACTERISTICS).

 

In the Pin functions, it says:

 

2.5 V to 3.3 V Supply for the AUXDAC and General-Purpose Output Pins.

 

 

so, does that mean if I want the GPOs & AUXDAC to function, the min VDD_GPO supply is 1.3V or 2.5V?

 

Thanks

-Robin

Outcomes