AnsweredAssumed Answered

HMC536 Control Voltage Spec

Question asked by Kevin.G Employee on Dec 10, 2014
Latest reply on Dec 11, 2014 by Kevin.G

With the HMC536LP2E and HMC536MS8G the datasheets give a table for the control voltage, but right above the table is a comment that says "*Control Input Tolerances are ± 0.2 Vdc".  What does this mean?  I'm more familiar with CMOS logic specs where VIL is a maximum voltage and VIH is a minimum voltage.  Does this mean for a logic low the control voltage needs to be below +0.2V (VIL max) and for a logic high that the control voltage needs to be above 2.8V (VIH min)?

 

control voltages.png

Outcomes