AnsweredAssumed Answered

Simlink AD9364 Transmitting not all time

Question asked by Storm21110 on Dec 5, 2014
Latest reply on Dec 29, 2014 by ACozma

Hello

 

Im using simulink and your model ad9364_sim.slx . It works, but on spectrum analazer (when i use it in span=0 MHz like power detector) I see, that tx power has period like 200-300 ms, then 50ms it has no transmitting. 50ms is fixed time, when I change frame size it have effect only on tx frame length (it would be about 500 ms - but I can`t see directly dependent with frame size: time changed, but not with the same coefficient), but delay 50 ms still the same.

 

What is it? How can I transmit all the time? Maybe it is in iio server?

Network is 1Gbps and I use only 20Mbps.

Thanks.

Outcomes