AnsweredAssumed Answered

ADL5391-Evalz as high frequency multiplier

Question asked by Sam87 on Dec 1, 2014
Latest reply on Dec 3, 2014 by jdobler

Hello,

 

I need a circuit which allows the multiplication of two high frequency data signals (up to 1 GHz). Is the ADL5391-EVALZ able to handle this? Do I have to make any changes at the circuit before starting (e.g. remove resistors, capacitors,…) or is the evaluation board ready to use out of the box?

The idea is:

Supply +5V to the board, set the first signal to XP, second to YP and get the output at WP, correct?

 

Thanks a lot!

 

Kind regards,
Sam

Outcomes