AnsweredAssumed Answered

ADE7878 sampling waveform - change sampling frequency

Question asked by DouglasPriamo on Nov 28, 2014
Latest reply on Dec 1, 2014 by hmani

Hello,

 

I want to use the ADE7878 as dual-purpose function: using this internal functions to provide some information about metering, and using the sample data for protection purposes (ex: 5051 Relays). I want to use a Sliding Window DFT algorithm with a integer "x" points per cycle - how to change the internal sampling frequency in the ADE7878 to a multiple of 60 Hz (example: 128 points per cycle, fs=7680Hz) to use sampling values in a Sliding Window DFT ? Change the oscilator input is a viable alternative?

 

Thanks in regard,

 

Douglas.

Outcomes