AnsweredAssumed Answered

ADV7842 Design Queries

Question asked by ayusman on Nov 28, 2014
Latest reply on Dec 5, 2014 by ayusman

Hi All,

 

I am looking for a receiver where I can support HDMI/DVI/Component/CVBS. I have come across ADV7842 which fits the requirements properly. Based on that I have a few queries.

 

1. I see that the maximum clock frequency is 170MHz. I need to support WUXGA I/P. Hence I believe I will not be able to capture WUXGA(1920x1200 @ 60). Please confirm.

 

2. If I use WUXGA with Reduced blanking, then the clock will be at 154MHz.In this case I believe I shall be able to capture the same using HDMI/DVI/Component interfaces.Please confirm.

 

regards

Ayusman

Outcomes