AnsweredAssumed Answered

Phase Detector for 12nSec square signals chip

Question asked by barresi on Nov 25, 2014
Latest reply on Dec 2, 2014 by rbrennan

Hi All,


I'm looking inside the AD product in order to choise the right chip to realize a quite Low Frequency phase detector. My goal is keep in phase two pulsed signals (Pulse duration= 12nS, Pulse amplitude range= +2 : +8 V, Pulse frequency range= 10KHz : 1MHz, Pulse shape = Square wave, Pulses delay range = 0 : 12 nSec.) The Pulses delay is digitally controlled => Each step delay is fixed = 100pSec.

 

 

[Edited for readability.]

Outcomes