AnsweredAssumed Answered

AD7150- Issue with data logging

Question asked by Aravind404 on Nov 24, 2014
Latest reply on Nov 28, 2014 by Aravind404

Hi all,

 

I am using AD7150 Evaluation Board, when I log data using "Log Data to File" for a capacitance of 10pF ceramic capacitor the value show in GUI is 10.1766 and the value shown in text file is 33775. When I short both the clips it shows a value of 17.7019 in GUI but shows 65535 in the text file which is logged. I used Cin range as 4pF.

 

How to convert the value shown in text file to the capacitance shown in GUI ???

 

I am attaching the text file generated when I used 10pf Ceramic capacitor.

Outcomes