AnsweredAssumed Answered

ZC706 ad9680_eval project

Question asked by mike.ericson on Nov 24, 2014
Latest reply on Nov 25, 2014 by mike.ericson

Hello,

 

Is the HDL project ad9680_eval/zc706 still being supported?  I tried both the hdl_2014_r1 branch and the master branch and neither worked.  From the log file, it looks like the port names on axi_9680_core changed at some point:

 

WARNING: [BD 5-235] No pins matched 'get_bd_pins axi_ad9680_core/adc_dwr'

WARNING: [BD 5-235] No pins matched 'get_bd_pins axi_ad9680_core/adc_dsync'

WARNING: [BD 5-235] No pins matched 'get_bd_pins axi_ad9680_core/adc_ddata'

 

Instead, these signals are split into _0 and _1 halves.

 

Also, there is this warning:

 

WARNING: [BD 41-597] NET <axi_ad9680_gt_rx_clk> has no source

 

Is there a way to sync the hdl repository so that this project can build?

 

Also, is there a pre-built image that can be loaded onto the ZC706 board?  I have the latest boot images and none match this project name.

 

Thanks in advance,

Mike

Outcomes