AnsweredAssumed Answered

AD9361's RF input power rating question

Question asked by ryan-tsai on Nov 24, 2014
Latest reply on Nov 25, 2014 by tlili

Hi Sir,

In the table 11 ,  we know the RF input  (Peak Power ) is 2.5 dBm which should be based on duty = 50 % .

And if the duty is changed to 10 %(Pulse)@@ and it should be withstood than 2.5dBm.

Did you have info. about duty V.S  input power rating? If yes , please give me about that.

 

Thank you!

 

(PS. The application is Radar so the duty is less than 50%)

 

 

Outcomes